This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV使用问题

Other Parts Discussed in Thread: LM3409HV, LM3409, LM3421

请问如何使用LM3409HV驱动西铁城电子CLL050-1825A1-303M1A2(200W 3000K)芯片?

电源输入60VDC 3.3A

如何利用PWM信号对芯片进行0%-100%调光?

灯具良好散热,可以达到200.5W。

请问是否需要利用两颗LM3409HV芯片驱动?

请问是否存在其他更合适的芯片替代LM3409?

 

 

  • 你好,按照CLL050的规格书,电流范围为0.2-3A,LED压降是48-63v;如果输入只有60v,所以很难确保输入足够大于输出。

    1.首先需要确认的是你的LED需要的电流大小;

    2. PMW调光可以通过外加PWM信号控制EN脚来实现, 调光频率最好至少是开关频率的1/10以下,详见规格书第12页

    3.LM3409HV可以驱动2A以上的LED电流;

    4.LM3409HV的输入最大电压75V,是比较适合驱动你这个LED模块的,但输入60V很难保证能驱动CLL050;

    5.如果要求输入电压即能小于又能大于输出电压,可以考虑一下LM3421,适用于升降压驱动LED。