This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133状态指示上拉电阻以及输入电压问题?

Other Parts Discussed in Thread: BQ24133

请假TI工程师两个问题: 1、BQ24133的state脚,对于上拉到VREF的电阻阻值有没有特殊要求?比如,建议上拉10K,我实际中用1K,是否可以?对BQ24133的其他功能会不会有影响? 2、12V输入,两串锂电应用场合。输入电压12V时,充电功能都OK,当把输入电压调高到13V,状态指示LED还是保持常亮,即正常充电状态,但13V输入电流只有0.03A,说明已经不再充电。电路图是用datas里面的典型电路。此现象是由什么引起?

 

 

  • 关于第一个问题,基准输出能力为最小35mA,因此不会有问题。但是,较大的电流会增加IC损耗。

    关于第二个问题,多半和输出电感饱和有关,建议提供详细信息。如IC和电感是否发热或有声音,是到13V就立即降电流还是过些时间等。

  • 感谢楼上朋友的回复。

    换成耐流大的电感后,现象消失。高电压下不能充电的确是由于电感饱和引起。

    前一版PCB到这一版,这部分就改动了state电阻,我还以为是这颗电阻引起。

    谢谢~