This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4501-SP: FB引脚电压高问题

Part Number: TPS7A4501-SP


Hi TI expert,

    FB引脚应该是固定1.2V,但是有时候会变成1.6V-1.7V,这样导致输出电压异常变高。
    现在测的5脚对地1.7V,4脚能到2.5V;

    这个可能是什么原因?

  • Hi

        ADJ脚的电压是输出电压荣国分压电阻获得,如果断开负载依旧偏高(排除来自负载的电压反灌),那就是LDO本身异常,可能已经损坏,建议更换确认(可以先排除一下反馈电阻是否有异常,不过一般很难损坏的?)

        如果确认芯片损坏,一般是输入过压,或者FB脚损坏导致。