This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92682-Q1: TPS92682&TPS92520的应用通讯问题

Part Number: TPS92682-Q1


你好,

我目前有个前灯驱动方案需要采用1个TPS92682的搭配3个TPS92520作为从机,MCU为主机进行SPI通讯,采用SPI for Multiple Slave Devices in Parallel Configuration的模式,但是我的SPI MISO波形很不正常,每个高电平信号爬坡均很慢,我3个92520根据规格书各自均进行了4.7K电阻上拉到5V,92682没有提及需要上拉没有进行上拉处理,另外SPI MISO没有放置任何电容,但是输出的MISO波形均不正常,导致SPI无法正常通讯,如图深蓝色线。

从上图可以看,RC时间有些大,而MISO上拉5V的等效电阻是=4.7K/3,而MISO没有外接电容,故而只能调整上拉电阻,我试过再并联一个电阻500-1K后,即等效电阻为3个4.7K再加一个500ohm并联,通讯才能正常。

针对这个问题,我目前的对策是否可靠呢?

是否有别人出现类似的问题,有没有什么其他好的解决方案啊。

急阿,盼望回复快一点。