Other Parts Discussed in Thread: TL431, LM358
LM358放大器与精密电压调整器TL431构成的恒压、恒流控制电路。
限压控制方面, 选用德州仪器公司生产的三端可调分流基准源TL431A。在应用中要选择传输系数和耐压较高的光电耦合器。另外需通过对TL431A进行分压,恒流控制方面,选用型号为LM358的运算放大器。
电流反馈信号通过LM358、二极管D6和光电耦合器反馈至OB2269的2脚FB端,再通过OB2269芯片控制输出电压,实现输出电流稳定在3A。
恒压电路工作原理:U2、ICIB、R6、R7、VD4、R10、U1组成电压控制环路。U2(TL431)是精密电压调整器,阴极K与控制极R直接短路构成精密的2.5V基准电压。R4是U2的限流电阻。2.5V基准电压由电阻R5送到ICIB反相输进端(6脚);而同相输进端(5脚)则由R6、R7的分压比来设定。若输出电压上升,则UR7电压也上升,该电压与反相端2.5V基准电压比较,7脚输出误差信号,再通过VD4和RIO变成电流信号,流进光耦中的LED,进而通过反馈控制网络控制一次侧PWM输出占空比,使输出电压工作在恒压状态。
恒流电路工作原理:U2、IC1A、R1、R2、VD3、R10、U1组成电流控制环路。R1是输出电流取样电阻,输出电流在R1上产生R1/IOUT的电压降。