This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【原创】基于LM2596的LED稳压电源

Other Parts Discussed in Thread: LM2596, LM358


LM2596开关电压调节器是降压型电源管理单片集成电路,能够输出3A的驱动电流,同时具有很好的线性和负载调节特性。固定输出版本有3.3V、5V、12V, 可调版本可以输出小于37V的各种电压。  该器件内部集成频率补偿和固定频率发生器,开关频率为150KHz,与低频开关调节器相比较,可以使用更小规格的滤波元件。由于该器件只需4个外接元件,可以使用通用的标准电感,这更优化了LM2596的使用,极大地简化了开关电源电路的设计。  其封装形式包括标准的5脚TO-220封装(DIP)和5脚TO-263表贴封装(SMD)。  该器件还有其他一些特点:在特定的输入电压和输出负载的条件下,输出电压的误差可以保证在±4%的范围内,振荡频率误差在±15%的范围内;可以用仅80μA的待机电流, 实现外部断电;具有自我保护电路(一个两级降频限流保护和一个在异常情况下断电的过温完全保护电路)

LM2596恒流电路,用LM358运算放大器比较电压结果控制其他电路是很常见的,实际很好用,也很简单,R6电流增加,电压就会升高,导致LM358输出反馈到LM2596电压调节电阻上,LM2596输出电压降低,电压降低电流减小,达到恒定电流目的。

给锂电池充电,假设LM2596输出电压为4.25V,直接给一块放完电的电池例如电压为3.3V左右充电,显然是有麻烦的,因为LM2596输出内阻比较小,接通电池瞬间电流将非常大,甚至超过3A,这样对芯片会发强热甚至烧毁,对电池也伤害大,如果不要求恒流的话,想用LM2596直接给锂电池充电,唯一办法是串联一个0.2-0.5欧限流电阻,这样保证在接通电池瞬间电流不超过2A,随后电池电压上升,电流稳定到0.3-0.7A左右,电池电压最后充到4.16V左右。

输出电流

 LED开关恒流稳压电源已经投入实际使用,且长期工作稳定可靠,该电路的成功设计,说明了利用市面常用DC/DC稳压器设计成高效的LED恒流驱动的方法的可行性,且取材广泛,成本低


该电路含有电压控制环路和电流控制环路两个环路。电压控制环路由运算放大器U2A、R1、R5组成,用于控制电源的最大输出电压。