大侠们,我用TPS54232D手工搭了个万能板,附件是原理图,
我们的输入是DC24V ,输出要的是5.3V 2A,
板子带负载后TPS54232D芯片冒烟,不知是什么原因,附件的参数是否有问题?求解,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大侠们,我用TPS54232D手工搭了个万能板,附件是原理图,
我们的输入是DC24V ,输出要的是5.3V 2A,
板子带负载后TPS54232D芯片冒烟,不知是什么原因,附件的参数是否有问题?求解,谢谢!
感谢 wei wang1的提示,
1. 我用示波器量TPS54232D第8脚和电感之间的波形,没看到1MHz的调制脉冲,不知是否正常? 芯片烧掉时,输出电流还没达到2A的,大概就1A左右。
2. 我的电感是用2A的,
3. 你输出5V,续流管用400V的?
原来的肖特基二极管B220A我用FR204代替了,FR204是applied reverse voltage of 4.0Vdc的,不明白怎么到400V了呢?
而原来的肖特基二极管B220A是applied reverse voltage of 4.0V D.C.,应该是可以替代的
Hi
如果计算到是5.6uF, 可以用到10uH,甚至15uH.
饱和电流2.5A以上即可。
还有就是在万能板上搭,容易造成短路,noise很大,甚至带不起来负载等问题,原因是电源芯片对layout要求是非常高的。