在选用TI的产品时候,我要考虑上电顺利,就采用延时,我知道可以用电感L或者电容C来起延时作用??这个延时时间怎么计算啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我要把这个TPS76901延迟0.225ms启动,我的这个接法对不对啊?这是对EN的定义介绍:A voltage of 1.7 V or greater on the ENinput will disable the TPS769xx internal circuitry, reducing the supply current to 1µA. A voltage of less than 0.9 V on the ENinput will enable the TPS769xx and will enable normal operation to resume. The ENinput does not include any deliberate hysteresis, and it exhibits an actual switching threshold of approximately 1.5 V.
我要把这个TPS76901延迟0.225ms启动,我的这个接法对不对啊? 这是对EN的定义介绍:A voltage of 1.7 V or greater on the ENinput will disable the TPS769xx internal circuitry, reducing the supply current to 1µA. A voltage of less than 0.9 V on the ENinput will enable the TPS769xx and will enable normal operation to resume. The ENinput does not include any deliberate hysteresis, and it exhibits an actual switching threshold of approximately 1.5 V.
TPS76901是低电平使能,大于或等于1.7v的电压会关闭TPS76901,如果低于0.9v会使能TPS76901, 如果要延迟0.225ms启动可以尝试通过RC+三级管的方式实现,
3.3v通过R给三极管基级所在的电容充电,一旦冲到0.6v左右,三极管打开,把原本上拉到3.3v的ENABLE控制信号下拉到地.R初步设为10K,C=0.125uF,不这种方式受三极管的开通阈值和电容电阻精度,温度影响较大,根据实际测试延迟时间选择电阻和电容值.
估算,RC = 秒, 1RC 时电容上电压为0.63电源电压。2RC时电容上电压为0.83电源电压。3RC时电容上的电压为0.95电源电压。
你需要的延时约为1.5RC = 0.225ms,则RC为0.15m,取R=10K,则C约为0.015uF,选个15-20nF的电容,能满足225uS的延时。
如果要精确的0.225mS的延时,建议使用专用的时序控制芯片。