This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电池保护测量问题BQ3050

Other Parts Discussed in Thread: BQ3050, BQMTESTER

我们正在测试BQ3050这款芯片,购买了TI一体的开发方案,采购了EV2300和一个测试版  Advanced bqMTester,根据数据手册及原理图,在电池连接正常地情况下,PACK+和PACK-输出应该是电池的串联电压,但我们测试的PACK+和PACK-之间输出电压为0,找不到原因,不知道是不是测试板bqMTester的问题,请帮忙解决
we have been using your products--BQ3050,there are some problems we can't solve,BQ3050 chips,according to schematic diagram and data sheets,which deserve to have a  Voltage Output when the cells discharge,however we tested the circuit board that was bought in America at recent days,therein,The voltage out between PACK+ and  PACK- is zero under the condition of the circuit ,other functions is formal
  • 您好。考虑到BQ3050带有保护电路,集成了充电MOSFET和放电MOSFET。你遇到的问题可能是因为放电MOSFET关闭了。解决办法是在BQ3050EVM测试板的PACK+/-之间加一个电源给电池充电。要注意电源电压要比你电池最高电压低,此外,只需要点几下充电即可,不需要长时间充电。

  • BQ3050集成了充电MOSFET和放电MOSFET的驱动,BQ3050EVM测试板上带有充电MOSFET和放电MOSFET。

  • 如果你测得电池最顶端有电压(电池正常)而PACK+/-没有电压,那么只需按一下BQ3050EVM左上角的WAKE按钮即可(此法无需在PACK+/-外接电源)。

    WAKE按钮按下的作用是给PACK+添加一个电压唤醒BQ3050,与前面所说的外接电源点充效果一样。