This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700做12V/0.5A 带容性负载启动困难

Other Parts Discussed in Thread: UCC28700

用UCC28700做了一个12V/0.5A 电源,其他指标都很正常,空带载电压稳定,平均效率80%,就是带容性负载启动起不来。

目前辅助电容用1uF/50V,(用2.2uF情况会改善些),空载辅助电压28V,额定负载外加470uF的电容开机就无法启动了,不外加电容带重载可以启动。

用示波器测试辅助绕组的波形,发现带电容以后,启动时的工作频率变低了很多,整个4毫秒的启动周期只有32个脉冲出来,辅助电压还没建立起来就停止工作了。

请论坛的高手帮忙分析一下,如何解决这个问题,我希望能做到满载启动可以额外带1000uF左右的负载电容,前提是辅助电容还是用1uF,谢谢!

  • 反激电源的辅助绕组输出电压和输出电压;都是遵守变压器匝比。因此:

    1)输出电容越大;建立电压时间越长,辅助绕组达到供电电压的时间也就越长。需要辅助电容维持启动的时间越长。

    2)输出电解的充电电流由一次电感储能决定,电流越大;充电越快;充电时间越短。

    所以;现在有两个方法可以用:

    1)如你所试;加大电容。在可接收的启动时间里,尽可能选合适的电容,满足负载要求。

    2)减小电流反馈电阻。在变压器和功率管和接收范围,适度增加电流。

  • 增大辅助电容是可以改善,但是50V/0805的电容最大也就2.2uF,并不能根本性解决问题,(板子空间有限只能用0805),况且规格书建议辅助电容不要超过1uF。

    这个是恒流电源,减小电流采样电阻输出电流就不是500mA了。

    UCC28700是QR芯片,不知道内部启动的时候是怎么工作的,启动工作频率是由什么条件决定的。

    我在想减小初级电感量是不是会有所作用,目前变压器的LP=1200uH,可减小电感会增加工作频率,减低效率