UCC3895振荡器定时电容选取什么电容好,频率在20khz到40khz,是云母电容还是其他什么电容?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC3895比较适合较高频率的设计,按照datasheet提供的公式Tosc=5Rt*Ct/48+120nS, 而Ct取值范围是100~880pF, Rt取值是40~120kHz, 可以Ct*Rt取值最大时得到最小频率f =1/(5*120k*880p+120n)=89.9kHz.
如果您的频率想做到20~40kHz, 推荐采用SYNC输入CLOCK的形式,这样会得到一个稳定可靠的振荡。