求推荐简单比较常用的12转正负12的线性稳压电源
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
12v的输入用什么比较简单的芯片能稳压出+12v或者+10v也行?你说的用降压芯片来做反向输出得到-12V,是怎么弄得,有没有具体的例子?我这对噪声、波纹比较敏感。
我这对噪声、波纹比较敏感,直接用DC-DC应该不行。能分开产生也行
Hi
做负电压前面必须有DC/DC转换,做正电压是可以直接用LDO的。
之前做得不好可能是你选择的LDO性能不是很好,你可以选择TI的低noise高性能的LDO,例如1A的TPS7A4700, 1.5A的TPS7A4501
负电压先用TPS54140或者TPS54160, 然后再用超低噪声、高 PSRR的1A TPS7A3301,
是不是把VOUT那个地方的地换成-12 v表示就行了,就不用接那个地了吧?电路其他地方都不用变吧,那个电容C0极性方向要变一下吗?
HI
是的,原本的Vout是接到GND, 然后图的Vout处实际是-12V. 电容不需要反向,因为上面的GND电压是高于下面的Vout -12V的。
TPS7A4700 ,TPS54140,TPS7A3301这些电源的输出电流的大小跟输入电压的大小有关吗?我如果用12V的输入产生10V的输出电压,那么输出电流是不是会很小?