如题:
想请教下前辈们,Bq76930 Cell数量软件配置问题,硬件连接已按规格书设置,但是读取软件SYS_STAT状态数据一直显示欠压,
UV_TRIP 配置为:0x97 默认
OV_TRIP 配置为:0xAC 默认
现实际电压为 3.2V左右
请问Bq76930是否有寄存器针对CELL的串联数有配置位。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
bq76930支持6~10节电池。
它不需要专门的寄存器来配置CELL的串联数目。具体的串联方法请参考datasheet 第40页“8.1.1 Configuring Alternative Cell Counts ”,里面详细说明不同节数电池怎么连接。
你的实际电压只有3.2V吗?是只有一节电池吗?
这个需要MCU或者上位机软件对寄存器进行清零动作才能恢复,所以对于930应用是需要配合MCU才能完成保护恢复。
BQ76930系列不需要专门的寄存器来配置节数,而是采用一个电压阈值来判断是否接有电芯,如果你已经按照规格书把不用的通道短接,那么ADC读到的电压肯定会小于UVminqual(0518)值,那么UV会被忽略,因为芯片认为这节电池是没有的。所以首先需要确认相应不用的通道是否可靠的短接。
另外,BQ76930系列的保护只能关闭MOSFET,恢复打开需要有软件来清楚相应的状态,所以BQ76930必须要配合一个外部的MCU来工作,这也是为了保护的可靠性考虑。
Rian peng 你好! 我也是在用BQ769306 我已经发了一个问题的帖子 麻烦你指导一下 谢谢了!
Hi Mingmo:
我正想用BQ76930 做6串的电池,能否发份CAD的电路原理图来参考下,谢谢!