This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295 大电流设置流程

Other Parts Discussed in Thread: BQ24295

 我用BQ24295作一个移动电源,用MCU来控制里面的reg,但是i2c地址 我采用默认的6B就是无法响应,只有用D6才可以工作,但是我在设置里面的reg时候发觉无法修改里面的reg,我本来设置的是3A电流,但是每次都会跳到800mA,我也关闭了看门狗,但是依旧会跳到800mA。不是硬件问题,因为我烧了一个别人写的程序,直接可以稳定在2A以上电流,因此不应该是硬件问题,但是由于那个程序只有bin文件,无法查看具体的设置流程,希望TI能帮忙给一个详细的BQ24295的设置流程。  还有用TI的EM板的USB转i2C,读取时候,地址似乎还是6B才可以读出,我都糊涂了,到底是怎么回事