Other Parts Discussed in Thread: BQ24295
我用BQ24295作一个移动电源,用MCU来控制里面的reg,但是i2c地址 我采用默认的6B就是无法响应,只有用D6才可以工作,但是我在设置里面的reg时候发觉无法修改里面的reg,我本来设置的是3A电流,但是每次都会跳到800mA,我也关闭了看门狗,但是依旧会跳到800mA。不是硬件问题,因为我烧了一个别人写的程序,直接可以稳定在2A以上电流,因此不应该是硬件问题,但是由于那个程序只有bin文件,无法查看具体的设置流程,希望TI能帮忙给一个详细的BQ24295的设置流程。 还有用TI的EM板的USB转i2C,读取地址又是6BH才可以,用电脑的软件直接配置BQ24295后,就可以维持在稳定大电流,实在搞不明白了,写入的数据我也做了验证,读取出来是对的,但是用电脑软件去查看,又不是之前写入的值,彻底晕了