This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于UCC28061 IC设计

Other Parts Discussed in Thread: LM358, UCC28061, UCC28060

使用UCC28061+LM358设计70W反激恒流LED驱动是否能解决普通单级PFC环路调整较慢的缺点?在输出短路,开环等保护上是否有改善?UCC28061是否能在各种条件下保持交错?另外,UCC28061抗干扰性是否能够胜任硅胶灌封环境?再有TI的咨询邮箱是什么啊?

  • 你好,我理解的你的电路架构是单级的交错反激PFC输出恒流控制。

    首先,UCC28061的推荐功率等级是100W-800W,具体你可以查阅到datasheet,你提到的70W电路方案,我们不建议采用UCC28061。

    ( www.ti.com/.../ucc28061.pdf )

    其次,你提及的几个问题我们可以一起讨论一下:

    1.通常我们的PFC是双环控制,你提到的环路较慢应该指外环,通常恒压输出PFC我们为了抑制100Hz纹波对后级电路的影响同时考虑为电流内环提供稳态的瞬时给定值,我们会把带宽做到几赫兹到几十赫兹,所以环路设计的指标不会有大的变动。

    2.保护策略上芯片支持过压、输入欠压、开环及输入电流冲击时的峰值电流限制等。

    3.UCC28060/1能严格保持180°的自然交错并联功能,TI在这方面有专利技术。

    4.对于灌胶环境,因为引入低频的寄生电容等不确定因素,我建议考虑在灌胶前的EMC测试中留有裕量,特别是RE测试。

    最后,对于TI的产品有任何疑问,可以发送邮件到TI的邮箱ti-china@ti.com,我们会及时处理。

  • Kevin Chen,你好,我最近在用UCC28061,但是非常奇怪,我观察两个MOS管的Vgs(驱动脉冲),在相对轻载时,其中一个Vgs几乎没有波形,只有零星会出现几个脉冲,当负载到300W左右时,两个驱动都相对变得密集起来,但是完全没有交错的现象,大部分时间甚至是同步的。请问这是什么引起的?(我的芯片4,5脚相连。)非常感谢。

  • 把PIN4连接到PIN15看看.