你好,我在我的电路中设计使用了TI的TPS73733,主要看中了它的低压差特性,按照数据手册TPS73701是可调的,于是我选择了TPS73733
固定3.3V输出的那款,按照数据手册典型的电路,我输入5V 的时候输出并不是3.3V,输出等于输入,不知为何,附件附上我的电路图,还请帮忙
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以测试一下TPS73733的Vin脚和Vout脚阻抗? 如果输入等于输出则已经击穿,建议
1.更换一个新的芯片,输入采用稳定的电源供应器,输出负载尽量小点(可以空载), 验证是否是输入电压过高或者电流过大导致的损坏), 看是否损坏?
2.如果新的芯片仍然这样,您可以在TI网站上申请样片,或者找TI授权代理商购买芯片,因为你之前的芯片可能是劣质产品。
TPS73733使用主要需要注意输入不要过压(小于6V), 因为是LDO, 功耗比较大,芯片背面的PowerPad需要充分与GND焊接,并利用宽广的GND铜箔散热,故layout上要注意。其次就是负载,避免过电流。