LM2596- 5.0 上电过冲 过冲到6~7V。
电路完全采用手册上的电路,冲击上电,电源24V。
500us内5V上电到5V,但之后过冲到6~7V!!!
PWM输出停震,等电压回到5V后再次起震。
过冲会导致负载损坏。
再网上找到其他人也反馈这个问题,但是没有解决。已知解决方法是将2596换为2576.过冲消失。难道有芯片BUG?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
请问冲击上电时的输出电感,输出电容是多少,负载电流多大?这些都是引起过冲的主要原因。
另外500uS电源就已经完成启动,启动有点过快,如果你的输出电感,输出电容,负载电流都比较大,过冲是很有可能存在的,另外LM2596是很老的芯片了,开关频率只有150kHz,这会使得输出电感和电容太大,有机会可以考虑LM22676,是比较新的同类型产品。
http://www.ti.com/lit/ds/symlink/lm22676.pdf