你好,
现在想做锂聚合物电池充电保护电路,该电池充电为两个过程3.7V-4.2V阶段为恒流充,4.2V为恒压充电阶段。
如果选择充电保护芯片
1.应该选择门限为4.2V的嘛?会不会到4.2V就关断了,丢掉了恒压冲阶段?
2.还是选择4.22V门限的关断芯片?
Zhetao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果使用4.2V的CV电压,充电保护芯片肯定保护门限不能选择为4.2V。一般的锂电芯选择的一次过压保护门限为4.28V,二段保护4.35V。
充电循环分为:涓流充电,如果BAT引脚电平低于2.9V,则充电器进入涓流充电模式。在该模式中,一般芯片 提供约1/10的设定充电电流,以便将电流电压提升至一个安全的电平,从而实现满电流充电。恒定电流模式,当BAT引脚电压升至2.9V以上时,充电器进入恒定电流模式,此时向电池提供恒定的充电电流。恒定电压模式,当BAT 引脚电压达到最终浮充电压(4.2V)时,进入恒定电压模式,且充电电流开始减小。当充电电流降至设定值的1/10,充电循环结束。
如果是使用4.2V的CV电压,充电保护芯片肯定保护门限不能选择为4.2V。一般的锂电芯选择的一次过压保护门限为4.28V,二段保护4.35V。
两节锂电池的充放电保护电路如图一所示。由两个场效应管和专用保护集成块S--8232组成,过充电控制管FET2和过放电控制管FET1串联于电路,由保护IC监视电池电压并进行控制,当电池电压上升至4.2V时,过充电保护管FET1截止,停止充电。为防止误动作,一般在外电路加有延时电容。当电池处于放电状态下,电池电压降至2.55V时,过放电控制管FET1截止,停止向负载供电。过电流保护是在当负载上有较大电流流过时,控制FET1使其截止,停止向负载放电,目的是为了保护电池和场效应管。过电流检测是利用场效应管的导通电阻作为检测电阻,监视它的电压降,当电压降超过设定值时就停止放电。在电路中一般还加有延时电路,以区分浪涌电流和短路电流。
一个正常的充电过程是不应该触发过压保护的。所以过压保护芯片是用来保护电池的异常过充的,一般来讲是会适当高于CV电压,比如4.25V。 对于4.2V的充电CV电压来讲,正常的充饱过程电池电压是不会超过4.2V的,当然,需要考虑下充电器的输出精度。
如果在充电阶段触发到了过压保护,通常是没有办法让电量达到100%的,因为你没有满足满充的条件。