有谁用过这个芯片,求指教,如何提升BQ24620的充电电流,按照技术文档上写的调节 ISET 两端的电压,但调节作用不明显,还请告知,不胜感激!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISET voltage range 0~2V 如果到最大还不够, 那就调节 Rsr.
The ISET1 input sets the maximum charging current. Battery current is sensed by resistor RSR connected
between SRP and SRN. The full-scale differential voltage between SRP and SRN is 100 mV. Thus, for a 10-mΩ
sense resistor, the maximum charging current is 10 A. Equation 2 is for charge current
技术手册上的公式是:Icharge = Viset / (20*Rsr),按照上面这个公式误差应该不会很大。您可以调电阻Rsr试一试。