目前想利用CSD95372BQ5MC这一类的驱动和降压MOS管集成的IC来实现高频下的同步BUCK,但是看该IC的数据表中关于推荐使用的说明中,输出电压最大只有5.5V,而占空比是推荐最大85%,输入电压推荐最大为16V,由于我的应用中输出仅5.5V是不够的,所以对这个地方的推荐有些迷糊。在我的应用中我希望IC的输出电压能在较大范围变化。还请大家指教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前想利用CSD95372BQ5MC这一类的驱动和降压MOS管集成的IC来实现高频下的同步BUCK,但是看该IC的数据表中关于推荐使用的说明中,输出电压最大只有5.5V,而占空比是推荐最大85%,输入电压推荐最大为16V,由于我的应用中输出仅5.5V是不够的,所以对这个地方的推荐有些迷糊。在我的应用中我希望IC的输出电压能在较大范围变化。还请大家指教。
输入电压12V,输出电压能到8V左右吧,因为我是要输出变换的,要能在1-8V左右吧
不知道你需要的输出电流有多大?如果电流太大的话,同步的MOS一般都需要外置,1-8V的下限才1V这种比较少。