请问: 对于TPS7A4901: 蓄电池24V输入,12V/0.1A的输出, 片子发热大不? 输出的纹波是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
负载为0.1A下,其功率损耗为1.2W,建议使用厚点的PCB铜层,并尽量使用敷铜的方式,加宽电源线与地线,且芯片
底部打几个过孔,以增加散热效果,布板可参考数据手册及附件中的说明。最小的输出纹波为16μV(RMS)(10Hz至100kHz)。