tps65217和AM3358一起使用,板子已经正常工作,所有外设都正常。问题是板子在工作十几分钟或更长时间后,SYS管脚会有一个向下的脉冲,使设备从新运行,电路中AC和usb同时供电时没有上述问题,但usb接头没有插上USB线时会出现上面问题。请帮助分析一下问题,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可能是SYS瞬间拉载, 而AC供电电流不够造成的, 量下AC输入端是否会同时出现与SYS管脚一样的向下的脉冲?
Hi,
查看下0x01h 寄存器的bit 3,2(AC input current limit)设了什么值?
00是100mA, 01是500mA, 10是1300mA, 11是2500mA,
如果设定的AC输入限流值低也会出现这样的问题.
我们这边配置到2500mA。不知道太大了是否也会有问题。这个电源芯片只供核心板,包括一个CPU,一个ddr,一个nandflash,一个I2c flash.
1.使用外加负载,看SYS到底可以抽取多大电流?
2.单独使用USB是否可以正常工作?接上电池是否可以正常工作?
3.对比USB下和 AC下,寄存器有何变化?
谢谢
AC 的电流是140mA。 再做后续测试时,板子坏了,不能继续下去,等新的板子回来再请教。