推荐一款芯片,恒流源(稳定度0.1%)提供控制电流
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用在霍尔元件上,减小温度误差——
恒流源及输入并联 电阻温度补偿电路——
温度变化引起霍尔元件输入电阻Ri变化,在稳压源供电 时,使控制电流变化,带来误差。为了减小这种误差,最 好采用恒流源(稳定度0.1%)提供控制电流。
输入电压范围是多少?输出电流是多少,要开关恒流还是线性恒流?
0.1%的精度是整个温度范围的精度? 还是初始精度? 整个温度范围未校准的精度达到0.1%是比较难的。
如果全温度范围要达到这个精度,需要做温度补偿,不断的校准。虽然实现麻烦点,但是可以达到要求的。
你好,
Victor Chen
我这边也需要一款开关恒流源、开关频率100MHz以上,输出电流范围1mA以内,我要用的是100uA以下的。主要用它来模拟光电二极管的电流的。有现成的开发板吗?