各位大侠,我在做一个镍氢电池的充电电流,有幸从网上弄到了一个BQ2002的样板电路,可搭建出来后,发现充电到不了12.5V,无论电阻怎样改动,只能到11.5V,怎么回事,请大侠们帮帮忙,谢了。我是通过24V开关电源充的,TS脚我拉的是高电平,只有BAT脚进行反馈,按照电路上的计算,BAT脚基本上在1.2V左右,可我改动电阻后,BAT脚都降到0.8V了,CC脚还是打开。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
充电开始后,bqZ2根据BAT和TS的输入来判断电池电压和温度是否正常,如果电池电压和温度超出快速充电的条件范围,bq2002将以TM端决定的速率开始涓流充电,反之,就开始进行快速充电。
看看是不是温度设定超出快速充电的条件范围了?