Other Parts Discussed in Thread: TPS40057, LM22676, TPS40060, LM5575, LM5576, LM5088
TPS40057能做18-36V输入电压,-5V1A输出的BUCK电路吗???该电路的模型是不是要求芯片输入电压范围≥41V呢???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有没有能输入电压范围比TPS40057大且满足我≥41V要求的芯片,替代TPS40057的芯片???
也可以参考TPS40060,输入范围10V到55V,和TPS40057是pin to pin的,参数基本一样。
过高的电压会导致过高的损耗,建议如果系统中有较低的电压值,可以从那个电压上再转-5V。