Other Parts Discussed in Thread: BQ76PL536A
你好,
我们在做太阳能的电能收集系统,需要高效的主动均衡方案,均衡电流最好能做到5A;
咱们TI有没有好的产品或者方案推荐?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ76PL536A
你好,
我们在做太阳能的电能收集系统,需要高效的主动均衡方案,均衡电流最好能做到5A;
咱们TI有没有好的产品或者方案推荐?
谢谢!
你好,TI有整套完整的主动均衡方案的,可以实现双向5A均衡电流。请问你们的方案是多少串一个电池模块?我可以给你推荐一套完整的方案。
你好,目前我们需要做主动均衡的是12串的,如果有4串的主动均衡方案最好能一并提供,谢谢!
对于12串的系统,模拟前端可以采用两个BQ76PL536A,一个BQ76PL536A可以支持6S,自动级联,电压精度可以达到1mV,而且集成二级保护,两个刚好12S。
对于主动均衡方案,你可以采用两个EMB1428和一到两个EMB1499.每个EMB1428可以支持七个通道的控制,EMB1499是一个双向DCDC控制器,目前这一套方案是业界最可靠最适合于量产的方案,结构简单。
对于MCU来说,如果要求可靠性高,可以采用TMS570序列,如果不要这么高的可靠性,M3,M4也都是可以使用的。
关于更多的技术细节,你可以联系你们公司对应的TI的FAE。
对于四串的方案,一个536,一个EMB1428和一个EMB1499就可以了。
你可以参考BQ76PL536A 这个芯片,用于 应用的 3 至 6 节串联锂离子电池监控器与二级保护 IC,支持所有化学成分
参见datasheet:http://www.ti.com.cn/cn/lit/ds/symlink/bq76pl536a.pdf
你好,
我看了你说的EMB1428和EMB1499,均衡电流由那些参数决定?请帮忙解答一下,谢谢!
均衡电流可以用外部电压对EMB1499来设定,在设计时候还需要考虑采样电阻,主变压器的设计,输出电感的选择还有MOSFET的选择。
EMB1428和EMB1499就是可以用于高串数的均衡的方案,因为这套方案本来就是设计用于EV和高压储能站应用的。而且这套方案非常的灵活,可以实现各种的配置。用于上百串的电池的均衡也是没有任何的问题的。具体的应用细节,我建议你直接联系你们公司对应的TI的FAE。因为这个很复杂,在这里三言两语很难说清楚。
你好 Richard,
谢谢你的回答,在最优的情况下EMB1499的最大均衡电流可以调整到多少呢?
就如我前面所说,均衡电流是由主变压器的设计决定的,你都可以设计到10A以上,只是相应的你的主开关FET,你的采样电阻,输出电感,还有通道控制FET就需要按照10A的应用来选择。本身1499并不限制你的最大均衡电流。
对于多芯锂电池管理IC,我在网站看到BQ77910,能支持10串。但为什么停产了,是这个片子本身有缺陷吗??