This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65130 电源关断问题

Other Parts Discussed in Thread: TPS65130

TI你好,

我在使用TPS65130的时候,采用了参考电路设计,输入5V,输出正负5V作为LCD屏的电压,发现在PSP脚拉高后,BSW立马拉低,输出立马会有正5V,但是在PSP脚拉低后,BSW立马拉高到5V,理论上来说pmos管si2323d是关断状态,si2323d的D输出应该是0,但是我们用示波器测试发现D端的输出是一个缓慢下降的过程,从5V下降到0付基本上需要20秒左右时间!似乎没有立马关断!我们采用物理开关替代si2323d,关断后,开关输出端,也就是原先si2323d会立马变0(虽然有个坡,但是很快,差不多几个ms),之后会有一个0.5v的上升,然后再慢慢回落到0v,请问是什么原因导致si2323d没有关断效果??

  • 写错了,不是PSP脚,应该是ENP脚

  • 按理来说只要VGS满足要求PMOS管就会通或者断。

    建议方案:

    1.先确定是由 PMOS 引起的,否则白废心机。拆走 PMOS 再量一下。(VGS=0时这个管子能关断吗?应该看一下手册是否如此。

    2.加的负载可能有问题。测试的时候,楼主有没有使用电阻作为负载呢?还是仅仅作假负载?断电的时候,直接通过钳位二极管进入电源,所以可能测出D端的输出是一个缓慢下降的过程。楼主不妨试试。

  • 首先,不知道你使用的si2323d是哪一家的?以VISHAY的为例,其关断电压要求-1V,0V可能不能完全关断。

    再次,看下你的负载情况,是不是很轻,导致电压缓慢下降。