+/-12V超低噪声稳压芯片推荐!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LDO的话,推荐以下方案。
|
Part Number |
Vin Range |
IOUT (A) |
Noise |
PSRR @1kHz |
Iq no Load |
Drop Out |
|
TPS7A30xx |
-3 – -36V |
0.2 |
15 µV |
72 dB |
61 µA |
216mV |
|
TPS7A49xx |
3 – 36V |
0.15 |
15µV |
72 dB |
61µA |
260mV |
|
TPS7A33xx |
-3 – -36V |
0.15 |
16 μV |
72 dB @10kHz |
210µA |
290mV |
|
TPS7A48xx |
3 – 36V |
1 |
16µV |
72 dB |
TBD |
216mV |