设计一款200V-1500VDC输入 24V 3A输出的辅助电源,准备使用1700V SiC做单管反激电路,TI是否有合适的控制器推荐?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TI提供了一个高达1000DC输入的参考设计: https://www.ti.com.cn/tool/cn/PMP41009
其实主要的问题在于MOS或者SIC的耐压,如果2个串联超过1500V,就可以做的。
目前准备使用1700V的单管,不存在两个串联,母线电压1500VDC,您指的是这种结构也可以吗?
使用这种串联电阻连接到HV引脚?
Hi
反激1700V也许有些偏低,选择2个1000V的管子按照上面设计应该是没有问题的。
如果你认为1700V足够的话,很多反激芯片都是可以的,主要就是芯片VCC供电难做。