HI,
请帮忙推荐芯片,谢谢!
1.芯片为车规,符合AEC-Q100标准;
2.支持尽可能多的快充协议,包括但不限于PD3.1,PPS,QC5.0,FCP,FCP,AFC,VOOC,苹果2.4A, BC1.2等;
3.尽可能过了UFCS认证;
4.尽可能集成升降压DC-DC功能;
5.输入电压适合车载12V,24V电源,输出功率不低于60W。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
请问你是要电源芯片还是其他方案,输入12~24V, 输出具体电压电流呢?
还是说你要的是typc_C的方案?