This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24610不能进入休眠

Other Parts Discussed in Thread: BQ24610

参考EVM板设计了充电管理板,接上电源可以充电,直接关闭电源时,BQ24610进入休眠模式,VREF无输出,但是,当输入电源慢慢降低到电池电压以下时,BQ24610则继续工作,STAT灯亮,指示在充电,这时关闭输出电源,STAT指示灯仍然亮,VREF输出3.3V, 请问,输入电源直接启动或关闭与电压缓慢变化对BQ24610有什么影响?为什么会出现以上问题?希望高手帮忙解决啊,否则,电池的电会被用光的啊。

  • 由于VCC由输入电源VIN和电池VBAT提供,而进入休眠的条件是VCC<VBAT+100mV,你可不可以测一下电源缓慢降低过程中VCC的变化,同时比较VCC与VBAT,看看是否满足休眠条件?

  • 你好,麻烦确认一个事情来确认该问题:当BQ24610继续工作时,输入端是否为稳定输出,PH PIN是否有正常的PWM波?

    如果确认是以上问题,则可能为充电IC的boost-back现象,可以通过以下方法解决:

    1. 确认输入端背靠背管子工作和设计正常;

    2. 确认BTST PIN的自举电容值为0.1uF/50V规格,且无电阻串联;