This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用tps65217b,大部分时候正常,但有时无输出,求解原因

Other Parts Discussed in Thread: AM3359

用tps65217b给AM3359供电,原理图参考Beaglebone

大部分时候加电,都是正常的,但有时tps65217b就不输出了。

外部电源供电5.1V,

正常时:

sys引脚4.9V。不知道是否降低的有点多,是不是负载过大?

不正常时:

sys引脚是0.6V,供电输出引脚因为都是从sys取电的,也都非常低

如果不正常时,把外部供电重启下,基本就好了。不正常状况出现的条件不明确,但比较频繁。

断开供电输出引脚中最早上电的LDO1,就正常了。

而且这路LDO1的电容比较容易击穿,甚至把这一路和CPU连接的引脚也击穿了,就是和地之间导通了。

是否这一路的瞬时电流很大呀