您好!我手里有3块BBB开发板,最近我在用开发板电池供电功能。即系统断电后,用电池抗一段时间,然后配置tps65217c在电池电压低于3.5V时候切断供电。即配置CHGCONFIG3寄存器DPPMTH[1:0]为00。
问题来了,我这只有一块核心板能在电池放电到3.5V时自动断电,即电池电压能维持在3.5V。而另外2块开发板电池电压降到2V左右才停止下降。不知为何。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!我手里有3块BBB开发板,最近我在用开发板电池供电功能。即系统断电后,用电池抗一段时间,然后配置tps65217c在电池电压低于3.5V时候切断供电。即配置CHGCONFIG3寄存器DPPMTH[1:0]为00。
问题来了,我这只有一块核心板能在电池放电到3.5V时自动断电,即电池电压能维持在3.5V。而另外2块开发板电池电压降到2V左右才停止下降。不知为何。
能稳定在3.5V的是硬件版本A5C,不能稳定在3.5V的硬件版本是A6。但两个版本用的都是同一款电源管理芯片
你可以仔细确认下,A5C和A6的硬件,软件差异在什么地方?即使使用了同一款电源管理芯片,其设置的电压点也可能是不一样的
软件一样,问题找到,是硬件问题。但不得其解.
A6的如下改动导致VDD_3V3A所使用的LDO4应该在断开时断不开。将A6如下改动复原回A5C。工作正常了。
1. Moved the enable for the VDD_3V3B regulator to VDD_3V3A rail. Change was made to
reduce the delay between the ramp up of the 3.3V rails.