Part Number: BQ24179
Other Parts Discussed in Thread: BQ25790
Hi tI Team,
请问BQ24179这颗芯片有没有最新的Layout指导?官网PDF里的图跟芯片PIN对应不上。


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请参考下面内容
There is no updated layout info. I will submit for datasheet update.
Below is a cutout from the BQ25790 EVM user's guide. BQ24179 is a downspin of BQ25790.

C24 (CPMID decoupling) and C26 (CSYS decoupling) are the most critical and must be placed on top of the IC on the same layer. C3 and C13 are the BTST caps. I recommend those be place on the bottom side of the board, connected with vias, instead of as shown above. That allows the CVBUS and CSYS caps to be placed closer. The inductor (partially shown at the top) is connected with vias but could be placed on bottom layer.