This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM3409N电流无法加大的问题!



 请问下:最近用LM3409N做输入22~26V   输出19V/2.45A的电路,在输出1A电流的时候频率是400K左右,但是电流再加大频率就变成60K左右了   而且MOS管很热!找了好久都没找到原因,元器件及电路都是按webench_design  做的!上面是线路图。求大神指点!

  • 您好,从原理图上来看在输入Webench_design时的输入/输出有点偏差了,从现在图上看是45V~50V输入和3.3V(单颗灯)的输出。

    附件是一份针对您应用的Webench_design文件(Vin=22~26V, Vo=19.2V, Io=2.45A),供参考。

     

    同时实际搭板实验时,请留意下电感除了感量外,其直流电流值也需与Webench design一致,测试/调试时建议看下开关波形。

    LM3409_19.2V_2.45A.pdf
  • 你好   开关波形在输出1A的时候是正常的  电流再加大的话开关频率直接下降到60K左右去了 ,电感是我用的15uH   你的意思是电感饱和吗,   我换了个很大尺寸的同样电感量的电感(在其它电源上拆的做70W电源的)还是这样!跟MOS有关吗?  我MOS用的是FQP17P10。

  • 1.请上传两种情况下的各种MOS管漏极和芯片PGATE引脚的波形,以做进一步分析。

    2.检查占空比的变化,看是否正常。

    3.注意散热,包括芯片的thermal PAD, 电感,二极管,MOS都要注意损耗是否超过要求,损耗较大注意散热。