This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

+-24与+-15V的转换问题



我的板子上需要+-24V,+-15V +5V 和+3.3V的供电。+-24V电流最大,最大不超过4A。+-15V的最大不超过1A,5V是给ADC用的,很小几十个毫安。3.3V是给MCU,也是几十个毫安。我们现在可以提供+-24V或者+-15V的电源,电流比较随意。

我的问题是,TI有这种集成的电源模块吗?可以通过+-15V或+-24V外部电源产生板子上的所需的所有供电?如果没有集成的,能否有一些组合的方案?

我是同过+-15V升压去产生+-24V好还是降压去产生+-15V更好?直觉觉得降压的更好一些。

不好意思,电源小白,原来都用现成的开关电源。谢谢各位了。