This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61081使用问题



首先,我的电路图如下:

电路目的,是5V输入,24V输出。

该电路结果:当时空载时,输出为24.2V,是我设计的输出值;但是当我接上负载后,电压只有6.5V,而且还听到吱吱的响声!我的负载是激光测距仪,电流最大100ma,也符合要求呀,不知道原因!