我使用LP2992IM5-5.0时,这是一款输入电压可调节,输出固定不变5V,但是我把输入电压从6V调到7.5V,输出电压可以输出5V,再把输入电压向上调节时,输出电压就变为0V,外围电路按照资料设置,但是调节外围电路的电容,也不能输出5V,而是0V,已经搞坏了两个芯片了,很是郁闷。请教高手解答,谢谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用LP2992IM5-5.0时,这是一款输入电压可调节,输出固定不变5V,但是我把输入电压从6V调到7.5V,输出电压可以输出5V,再把输入电压向上调节时,输出电压就变为0V,外围电路按照资料设置,但是调节外围电路的电容,也不能输出5V,而是0V,已经搞坏了两个芯片了,很是郁闷。请教高手解答,谢谢!!
Hi YongZhao,
请问LP2992的输出负载电阻,或者说负载电流是多少?测试是在空载的情况下吗?
在正常工作时,芯片是否会发烫?
谢谢。
Hi
用示波器测试一下你改变输入电压是输入是否出现不稳定的现象,例如Spike? 这个会导致过压损坏
谢谢了,已经好了,又从另一家拿的货,就好了,可能原先的厂家提供的样品是假的。