This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ24195怎么设置升压输出?我的输出一直没有5.1V
1. BAT电压要大于BATLOWV阈值
2. VBUS要小于VBAT+VSLEEP
3.OTG引脚为高电平,且REG01[5:4]=10
非常感谢!后来我在手册上看到了,第一次看的时候,看到那里有点晕,直接跳过了,所以就不知道怎么弄
您好!按照这种方式配置了后.
1.BAT(4.15V)>BATLOWV(3.0V)
2.VBUS(1.13V)<BAT(4.15V)
3.OTG=VSYS(3.98V),REG01=0x2b.
PMID处的电压是3.67V,没能升压上去.想请教下我的问题会出现在哪呢?先谢谢了.
我的现在也是这样,同求答复