Other Parts Discussed in Thread: TPS60400, OP07
不是输入正电压,输出负电压 ,我做出来的输出怎么是0V呢?求指导 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.请问设计的是参考线路中的哪一个?输入多少V,输出多少伏?
2.注意检查不要虚焊了,
HI
REP3330如果是一个3V的电压源,输出到TPS60400的输入只有2V,电流还被1k的电阻限制,一旦后端工作,1k电阻上压降增加,TPS60400的输入电压肯定会低于1.6V而无法启动芯片,除非1k电阻上电流小于1.4mA左右,也就是说TPS60400基本上没有带载能力。
谢谢您的回答!嗯嗯 这个和我想的一样 最后我也想到了这个原因 所以我在2V后面 又接一个 由OP07做成的电压跟随器 这样就可以达到2V的输入 同样输出得到-2V的电压。不知道您还有其他的解决方案没?
Hi
为什么不把REF3330替换成能输出2V的基准源或者LDO?