使用27510一定需要ev2400/2300进行参数的配置吗?可以只使用单片机进行配置吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以用单片机对 bq27510进行配置,支持标准的I2C。
TI提供了用MSP430 MCU I2C读写Gauge的示例代码,你参考下:http://www.ti.com.cn/analog/cn/docs/litabsmultiplefilelist.tsp?literatureNumber=slva413a&docCategoryId=1&familyId=412
用EV2400/EV2300的话就可以利用TI提供的非常便捷的上位机软件进行配置。
详细的寄存器介绍及配置方法不在数据手册里,在另一篇技术文档里:http://www.ti.com/lit/an/slua559/slua559.pdf
配置的作用是令bq27510能根据电池正确地工作。使用单片机进行配置的例程请参考上面说的MSP430例程。单片机与bq27510的连线只需要I2C连接,所以如果你用单片机自带的I2C模块就将把两者的SDA/SCL连接起来即可。
BQ27510基本参数可以用I2C配置,但是电芯曲线CHEM-ID等内容没有开放出来,只能通过TI的上位机配置评估套件EV2300/EV2400进行设置。