This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54428DDA 输出电压随着输出电流的增大而减小,什么原因,怎么解决?

Other Parts Discussed in Thread: TPS54428

电路和推荐设计完全一致 ,输入10V,输出3.3V,4A,当 输出2A时,电压为3V,当 输出4A时,电压为2.7 V

DC output.pdf
  • 楼主,首先,检查一下电源输入是否限流了。另外,TPS54428能够流过的最大电流是4A,看一下SW波形,有可能触发到了限流。你是缓慢往上调负载时,输出电压往下掉,还是直接带载到4A时电压掉下去的?

  • 电源输入采用10V,最大电流3A。

    SW 波形在输出1A 左右时,频率为702K左右,占空比33%,在输出3A 左右时,频率为690K多,占空比35%,在输出4A 左右时,频率为690K多,占空比37%,

    负载无论直接加到4A,还是缓缓上调负载,都会出现输出电压下降的现象;而且在负载为200mA时输出电压就已经下降到3.21V,也就是说负载逐渐增加导致输出电压逐渐减小。

    电感选用市场采购的Coilcraft XAL6030-222ME(3.3V输出), XAL6030-332ME(5V输出)。

  • Hi

       换一个类似规格电感试一下,主要电感的饱和电流要足够。

       其次主要一下layout,主要是PowerPad 焊盘的PCB GND散热面积要尽量的大,用于给芯片散热。

  • Hi

       如果最大要4A输出,建议选择6A以上的电感,甚至按照芯片的swicher 规格来选择6.8A.