BQ40Z50-R1的FUSE引脚,在二次保护时可以永久失效吗,要怎么设置呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ40Z50-R1芯片的FUSE引脚,在二次保护时可能会永久失效,需要避免过大的电流冲击。为了避免FUSE引脚永久失效,可以在设计电路时采用额外的过流保护电路来降低FUSE引脚受到过大电流冲击的风险。例如,使用快速恢复二极管、熔断器等,以限制电路中的电流和电压变化。此外,还需要注意电路布局和维护,确保FUSE引脚与其他高电流元件(如电机、继电器等)保持一定距离,从而避免不必要的电流冲击。
关于如何打开BQ40Z50-R1芯片的PF功能,首先需要将PF_EN引脚设置为高电平,并且在寄存器中进行相关参数配置。具体的步骤如下:
配置完成后,芯片应该能够在电池电压过高或温度过高时,通过开关控制器来控制预充电FET的导通和断开,以保护系统安全。
当温度超过保护温度时,PF状态位SOT未置位可能与芯片引脚的PTC和PTC_EN接地有关。在使用NTC检测温度时,需要将PTC和PTC_EN引脚连接到NTC电阻上,并在芯片寄存器中进行相应参数配置。如果PTC和PTC_EN引脚未正确连接或者未正确配置寄存器,可能会导致PF状态位SOT不置位。因此,请确保PTC和PTC_EN引脚的连接和参数设置正确,以便正确检测温度并置位PF状态位SOT。