This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED照明

Other Parts Discussed in Thread: LP55231

目前我们用LP55231驱动RGB灯,绿色和蓝色灯可以正常驱动点亮,但红色灯无法点亮。我们根据LP55231的数据手册采用的是LP55231的D7,D8,D9引脚来驱动红色灯。我们采用的是3.3V供电。按照数据手册里3.3V供电时可行的。但是无法点亮红色灯

  • 您好,无法点亮是完全无法点亮么?

    用万用表检查下D7,D8,D9脚的电压,看是否为高电平?

    用哪个管脚驱动那种颜色的灯不重要,重要的是通信控制成功,灯是好的。

  • 您好,3.3V的供电是OK的,因为红色LED是导通压降最小的(2V左右),故用3.3V, D7/D8/D9来驱动OK。

    建议两方面看下:

    1. 红灯的程序配置是否OK(电流/PWM调光部分),规格书中各寄存器的描述及最后典型应用的例子可供参考。

    2. 顺便看下3.3V供电是否稳定,确认下是否有带载时有电压跌落等的情况。

  • 从光源区别来说,红色LED的Vf要低一点的,

    红绿蓝三种LED芯片的VF值不一样,红的是1.8V到2.2V,绿和蓝是2.8到3.3V不等
    留意下是否负载的原因