This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5907: 选用DSBGA封装的器件,定压2.5V的LP5907UVX-2.5的输出电压问题

Part Number: LP5907


LP5907UVX-2.5这个器件会随着负载电流的变化,输出电压有差异吗?

我们测试不带任何负载时的输出电压时2.488V,加100mA负载后,LDO输出管脚处输出电压为2.476V,输出电压降了十几mV,这个指标是正常的吗?

此封装的最大输出电流为250mA,那么是否输出电流更大,这个电压会降的更低?

  • LP5907UVX-2.5是一款低压差线性稳压器,其输出电压随着负载电流的变化会有一定的波动。这种波动是由于内部反馈机制对负载的响应速度限制而引起的。因此,当负载电流增加时,输出电压会下降。

    在您的测试中,输出电压降低十几mV的情况是正常的。不过,如果您需要更高精度的电压输出,您可以选择其他型号的LDO芯片或采用外部稳压器进行补偿。

    另外,请注意LP5907UVX-2.5封装的最大输出电流为250mA,并不保证该电流下输出电压的精度。如果超过最大输出电流,则可能会导致输出电压降低更多。因此,在设计时,请确保负载电流不超过规格书中所述的最大输出电流。

  • Hi

        回复如上。