我用的是BQ20Z655-R1电池检测芯片,自己做了一些配置,电池在芯片的检测下充满电,然后进行低温放电试验,刚开始放电正常,bq Gas Evalution 界面上显示的电量也是正常,但是当温度降到-20℃左右后,bq Gas Evalution 界面上显示的电量突然就变成0%了,并且charging status中的XCHGLV也被反复置位和重置,放电出现异常,时断时续的,BQ20Z655-R1控制的LED闪烁也变得异常。但是当电池温度恢复室温后,电量又会出现。是不是DF中的某个数据设置的不对啊?