This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3060的RSOC



能不能在RSOC为0后继续放电?

为什么RSOC为0继续放电一段时间后,开始充电了,Remaining Capacity不能正常增长了,一直是0?

  • RSOC 为0后继续放电,会照成电池过放,这个“过放”不一定是物理意义上的过放,是指的电量计计量芯片内部算法认为的“过放”,及RM<0。

    RSOC为0后继续放电,电量计芯片的RM<0. 因此在充电时,RM 需要等待一段时间从负值慢慢增长到0,再继续往上增长。显示出来的RM会一直显示0。

    如果遇到这种情况,请合理设计电池的EDV0点,使电量计RSOC = 0 时,系统能够关机。

  • 谢谢!我还有一个情况,当我放电到RSOC为0后,继续放电了一段时间直到电压低于某一阀值,然后标定RM为0,然后充电,结果很长时间RM一直为0,RSOC也为0,能不能帮忙分析下芯片内部逻辑?