Other Parts Discussed in Thread: TPS62175, LM2586, TPS54061
电源输入为9V
1.要求输出负9V为运放供电,用于音频信号放大(非功率信号),输出电流小于100mA
2.成本在5块人民币以内为佳
3.噪声尽量低 占用PCB尽量小
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可能因为电感的一致性不好,你可以交换电感测试,看问题是跟着电感走还是跟着板子走
jiaxin li 说:整个系统是+9V电源适配器供电,纹波大致在50mV以内,如果双路±9V能进一步降低+9V的纹波是最好的了。目前试过的intersil的ISL85415,负压的纹波大致在40mV以内,不过有个问题,电路中的电感有时会啸叫,啸叫会耦合到输出信号中,十分不解。而且手工焊接了三台样机,两台在多次上电后噪声会变大,另一台却十分稳定。后面希望能在性能与成本中做个折中,所以想多尝试几种方案。40mV的纹波基本就可以接受了,目标是做到30mV以下。