Other Parts Discussed in Thread: LM3429, LM3421, TL4242
需要同时驱动8颗LED,这些LED波长不同,产品说明上注明这些LED电压在3.4——3.8V之间,输入电压现成的有12V,需要350mA电流,请问哪种芯片最合适,最稳定。十分感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,想请教几个问题,然后才能给你推荐合适的方案:
1.这些LED是否可以串联驱动?
2.是否需要调光?
3.是否关注效率?
4.对噪声是否有要求?
谢谢
如果你的噪声有要求的话,,TI好多种IC都可以做到,主要看你控制价格方面,,高高效率的东东,,成本上肯定会高的。
LED是需要恒流驱动的哦,你8颗LED,要弄清楚串并结构,比如你是4串2并,那你LED的电压乘以4,就是你电源输出的最低电压,然后电流设计成350/2=175mA,就可以了。 或者你8串1并,那就是LED电压乘以8,就是你电源的最低输出电压,电流就是350mA,至于选什么芯片,跟你产品的要求有关系,比如要不要过EMC,比如成本有没有要求,输入电压是多少,要不要支持调光等等,
所以你先确定你的要求,才能选驱动方案的,驱动方案,TI就有N多种,更别提市面其他厂家的IC了。
1.如果输入电压够高,建议使用线性LED驱动器,TL4242,噪声小
2.如果输入电压不够高,建议采用boost + 线性恒流源实现,效率高,噪声小。
谢谢